Technical FAQs

Ask a Question

Will the PK3GTA through PK27GTA Equipment Ground Bars accept either solid or stranded conductors?

Issue:
Product Features

Product Line:
QO and Homeline Load center Ground bars

Environment:
Wire size and type

Cause:
Application

Resolution:
Yes, the ground bars will accept either solid or stranded conductors. SEE THE TORQUE LABEL ON THE LOAD CENTER OR IN THE GROUND BAR KIT FOR WIRE SIZES AND TORQUE.


CTA-ID : 2055432
Was this helpful?
What can we do to improve the information ?