Technical FAQs

Ask a Question

Are the Tesys LRD overloads equipped with both Normally Open (NO) and Normally Close (NC) contacts, and if so, how are they marked ? <br /><br />

Yes. The Normally Open ``alarm`` contact is between terminals 97 and 98 . The Normally Closed ``overload`` contact is between terminals 95 and 96 .


CTA-ID : 2055540
Was this helpful?
What can we do to improve the information ?