Technical FAQs

Ask a Question

What is the difference between a PK15GTA and a PK15GTAFT?

The PK15GTAFT`s only function would be to have a larger separate lug to run wire from one ground bar to another. The lug assembly is a piece of bus bar with two lugs one mounted on each end and space in the middle to put the actual PK15GTA ground bar.

CTA-ID : 2055561
Was this helpful?
What can we do to improve the information ?