Technical FAQs

Ask a Question

What are the dimensions for a QOC40UFL cover?

This longer cover overhangs the enclosure approx. 2-3/4 inches at the top and approx. 3.0 inches at the bottom. The length of the enclosure is 33.78 inches high and with the overhang at the top and bottom the total height is 39.18 inches x 15.44 inches wide.

CTA-ID : 2054961
Was this helpful?
What can we do to improve the information ?