Technical FAQs

Ask a Question

Can the MPH42200 be used in a commercial application?

Yes, as long as it is used within its applicable ratings:
120/240Vac 1 Phase/3 Wire
Suitable ONLY for use as Service Equipment
400A Main Lugs
200A Maximum Tenant Breaker
22,000 AIC Maximum Short Circuit Current available

Always check with the local utility company for their approval before purchasing or installing this equipment.


CTA-ID : 2055444
Was this helpful?
What can we do to improve the information ?