Technical FAQs

Ask a Question

Will a PK23GTA-L Equipment Ground Bar accept either solid or stranded conductors?

Yes, this ground bar will accept either solid and stranded wire. However, there is an exception if terminating two ground conductors of different sizes. If terminating a #14 CU and a #12 CU; a #12 CU and a #10 CU; a #14 CU and a #10 CU or a #10 AL and a #12 AL, stranded conductors cannot be used. This information pertains only to the ground bar, not the larger individual lug also supplied with the kit.


CTA-ID : 2055441
Was this helpful?
What can we do to improve the information ?