Technical FAQs

Ask a Question

Does the EIK031 OR EIK032, Electrical Interlock Kits, provide Form C contacts?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Accessories

Cause:
Application

Resolution

No, the kit EIK031 provides Form Z contacts, 1A (NO) and 1B (NC). The 9007AO1 snap switch is used in this electrical interlock kit to provide the contacts.

No, the kit EIK032 provides Form ZZ contacts, 2A (NO) and 2B (NC). The 9007CO3 snap switch is used in this electrical interlock kit to provide the contacts.


CTA-ID : 2055585
Was this helpful?
What can we do to improve the information ?