Technical FAQs

Ask a Question

Will wiring the PF (ready to close) switch in series with the XF (closing) coil inhibit or defeat the anti-pumping feature of the breaker?

Yes, it will. Anti-pump is in effect only if continuous voltage is applied to the coil and the pf switch will interrupt it and allow it to pump.

CTA-ID : 2054212
Was this helpful?
What can we do to improve the information ?