Technical FAQs

Ask a Question

Can the optional lug AL800MA7 fit on the SL800 sub-feed lug kit?

Issue:
Optional lugs

Product Line:
Panelboards

Environment:
I-Line

Cause:
Sub-feed lug kit

Resolution:
There is some interference with getting the hex tool in the wire binding screw. The molded case would need to be filed about 3mm to make room for the hex tool.

This lug is suitable for 2-500-750kcmil conductors per phase.


CTA-ID : 2054167

Was this helpful?
What can we do to improve the information ?