Technical FAQs

Ask a Question

8538SEA23V06 - what type fuse does this take?

Configured from factory to accept Class H, J, K or R fuse types - however, this device is not supplied with Class R rejection pins; if Class J fuses are used, customer will need to re-position the fuse base.


CTA-ID : 2054153
Was this helpful?
What can we do to improve the information ?