Technical FAQs

Ask a Question

Are the QOU14100JBAF, QOU14100JBAR, QOU14100JBAL, QOU14100BAFB, QOU14100BALB or, QOU14100BARB Jumper Bar Assembly suitable for both single phase or three phase voltage systems?

Issue:
Application:

Product Line:
QOU Jumper Bar Assembly

Cause:
Clarification of application

Resolution:
These QOU Jumper Bar Assemblies are only suitable for use single phase voltage systems.


CTA-ID : 2054061
Was this helpful?
What can we do to improve the information ?