Technical FAQs

Ask a Question

What is the difference is between a QON3B and QON3BRT OEM mounting base?

Product Features

Product Line:
OEM Mounting Base

Product feature differences

The QON3B is provided with mechanical lugs to accept the incoming conductors. The wire range for the mechanical lugs is #12 - #1 AL or CU. The QON3BRT is provided with 12-24 studs to accept ring terminal connections. 

CTA-ID : 2054600
Was this helpful?
What can we do to improve the information ?