Technical FAQs

Ask a Question

What are the repair parts for a QO612L100DTS, Series G3, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 40553-453-51(which replaces the obsolete 4055310851).
Interior Assembly - 4055328450
Neutral Bonding Screw - 4028329750
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
NOTE: Labeling is not supplied on the replacement cover and the cost of the replacement cover may be close to, or exceed, the cost of a new device. You may want to consider buying a new device and use the new cover on the existing device.

Revised 08/10


CTA-ID : 2054741
Was this helpful?
What can we do to improve the information ?