Technical FAQs

Ask a Question

Does the UL listed MSC mounting base for Multi-9 breakers have DC ratings?

Yes, it is rated for 240 Vac and 125 Vdc.


CTA-ID : 2054735
Was this helpful?
What can we do to improve the information ?