Technical FAQs

Ask a Question

8536 starters, Sizes 00, 0 or 1 - looking for ground lugs. What is needed?

Ground lugs are provided only on combination starters. No provisions for ground lugs for Class 8536 starters - if required, customer will have to do on his own.

CTA-ID : 2053951
Was this helpful?
What can we do to improve the information ?