Technical FAQs

Ask a Question

Are the dimensions for an AP2508G10ST and APH2508G10ST the same?

Yes, they both have the same physical dimensions of 4.34` x 5.88` x 120`.
The difference between the two is short circuit bracing which does not affect the physical dimensions of the busway.
AP2508G busway has a s/c rating of 50Kaic
APH2508G busway has a s/c rating of 75Kaic

CTA-ID : 2054807
Was this helpful?
What can we do to improve the information ?