Technical FAQs

Ask a Question

What are the repair parts for the H461DS, series F5? (may be shown as F05)

The repair parts for the H461DS, series F5 (F05) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)
-Line Base - one each of 40566-259-50 (left side base), 40566-235-50 (right side base), and 40567-028-01 (plastic connecting cam) (NOTE: arc suppressor not included)
-Load Base (requires 1 for left side, and 1 for right side) - 40566-150-50
-Line & Load Base mounting screw - 40205-151-01 (3 for each line base & 2 for each load base)
-Arc Suppressor Assembly - 40566-355-50 (requires 1 for left side, and 1 for right side)
-Arc Suppressor mounting screw - 40205-145-01 (1 required per arc suppressor)
-Lug Assembly - CL0306F (includes 6 lugs)
-Mechanism Assembly - 40566-469-50 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 40566-998-50
-Cover Interlock Defeat Coupling - 40566-997-50
-Handle Assembly - 40567-798-50 (also recommend replacing Lockplate Gaskets)
-Lockplate - 40566-812-01 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 40503-228-02 (2 required)
-Lockplate mounting screw - 21949-001-01 (2 required)
-Ground Lug - 40251-016-52 - (2 total required)
-Ground Lug Mounting Screw - 40205-135-03
-Fuse Pullers - FPK0610 (1 required for each line base)



CTA-ID : 2054774
Was this helpful?
What can we do to improve the information ?