Technical FAQs

Ask a Question

What are the repair parts for the H463DS, series F5? (may be shown as F05)

Repair parts

Product Line:
Heavy Duty Safety Switch


The repair parts for the H463DS, series F5 (F05) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)
-Line Base - one each of 40567-764-50 (left side base), 40567-758-50 (right side base), and 40567-028-01 (plastic connecting cam) (NOTE: arc suppressor not included)
-Load Base (requires 1 for left side, and 1 for right side) - 40566-151-50
-Line & Load Base mounting screw - 40205-151-01 (3 for each line base & 2 for each load base)
-Arc Suppressor Assembly Kit - HAS0610F (2 required)
-Lug assembly - CL10F (includes 6 lugs)
-Mechanism Assembly - 40566-469-50 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 40566-998-50
-Cover Interlock Defeat Coupling - 40566-997-50
-Handle Assembly - 40567-798-50 (also recommend replacing Lockplate Gaskets)
-Lockplate - 40566-812-01 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 40503-228-02 (2 required)
-Lockplate mounting screw - 21949-000-01 (2 required)
-Ground Lug - 40251-018-51 - (2 total required)
-Ground Lug Mounting Screw - 40205-148-01
-Fuse Pullers - FPK0610 (1 required for each line base)

CTA-ID : 2054769
Was this helpful?
What can we do to improve the information ?