Technical FAQs

Ask a Question

Are hangers available for the Raintight Trough NEMA 3r RDB122, RDB123 RDB125 and RDB126?

No. However, there are mounting holes on the back side of the trough to attach to a wall.

CTA-ID : 2054810
Was this helpful?
What can we do to improve the information ?