Technical FAQs

Ask a Question

What is the contact block replacement for a XY2CE switch?<br /><br />

The XE2SP2151 is a snap action block, 1-NO and 1-NC contact for the XY2CE and XY2CH normal action momentary contact cable pulls switches only. This contact block is not replaceable in the Emergency Stop circuits which use Slow make, Slow break contact blocks.

The XESP2151 was the original block for this device, with a one color label. Current contact block is identical in design, but with a 2 color label.


CTA-ID : 2054785
Was this helpful?
What can we do to improve the information ?