Technical FAQs

Ask a Question

Do we have barriers available for use with our current style, NEMA 1 Wireway?

Yes, barriers used on NEMA 12 units can also be used on NEMA 1.
Example; We currently have available for the following:
Size Part Number
4`` x 4`` LJB45B
6`` x 6`` LJB65B
8`` x 8`` LJB85B
These units are 5ft. long and come with mounting hardware.


CTA-ID : 2054521
Was this helpful?
What can we do to improve the information ?