Technical FAQs

Ask a Question

What material is the XB4BT845, Non-Illuminated Emergency Stop Mushroom Head Push Button made of?

Issue:
What material is the XB4BT845,  Non-Illuminated Emergency Stop Mushroom Head Push Button made of? 

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
The head material is a Polyamid and the metal body made with Zamak.


CTA-ID : 2054507
Was this helpful?
What can we do to improve the information ?