Technical FAQs

Ask a Question

Can the core and coils be removed from a Model III substation on site?

Yes. Remove cables from lug pads. Remove ground strap from the transformer to ground. Remove the lag bolts. Remove the roof - drip hood and vent.


CTA-ID : 2054570
Was this helpful?
What can we do to improve the information ?