Technical FAQs

Ask a Question

What size conductors can be used with RPZF sockets?

The conductor information for the RPZF1, RPZF2, RPZF3 and RPZF4 is listed as follows:
Solid wire without cable end is 1 conductor: AWG 20-12 (0.5-2.5 mm2) or 2 conductors: AWG 20-14 (0.5-1.5 mm2)
Flexible wire with cable end is 1 conductor: AWG 24-14 (0.2-2.5 mm2) or 2 conductors: AWG 24-16 (0.2-1.5 mm2)
Flexible wire without cable end is 1 conductor: AWG 24-14 (0.2-2.5 mm2) or2 conductors: AWG 24-16 (0.2-1.5 mm2).


CTA-ID : 2054048
Was this helpful?
What can we do to improve the information ?