Technical FAQs

Ask a Question

Can the NQSFL2 be used in a NQOD panel in place of NQOD225SFL?

Issue:
Can the NQSFL2 subfeed lug kit be used in an NQOD panelboard in place of the obsolete NQOD225SFL?

Product Line:
NQOD panelboards that were sold and supported in the USA.

Environment:
Cross reference

Cause:
Since the NQOD225SFL is now obsolete, can the current NQSFL2 be used as a substitute in an NQOD panelboard?

Resolution:
No, there is no replacement for the obsolete NQOD225SFL.  The NQSFL2 is strictly for use in NQ panelboards and will not work in an NQOD panelboard. 








CTA-ID : 2054360
Was this helpful?
What can we do to improve the information ?