Technical FAQs

Ask a Question

<br /><br />What is the AIC rating of the main breaker in an HCN09521MN?

The main breaker is an FA36100. Ratings are:
25K AIC @ 240V
18K AIC @ 480V
14K AIC @ 600V


Revised 3/10/04




CTA-ID : 2054554
Was this helpful?
What can we do to improve the information ?