Technical FAQs

Ask a Question

Are the FA, 2 pole and 3 pole breakers rated for 10 kAIC or 25 kAIC at 240V?

Breakers that begin with the part number FA22 or FA32 are 240V breakers and have a 10kAIC rating at 240V. Breakers that begin with the part number FA24 or FA34, are rated for 480V, but may be applied at 240V, and when applied at 240V they have a 25kAIC rating.


CTA-ID : 2054552
Was this helpful?
What can we do to improve the information ?