Technical FAQs

Ask a Question

<br /><br />What is the wire bending allowance for the HCM1464-4M interior?

Wire bending allowances are (1) #1 - 600kcmil A./CU or (2) #2-250kcmil Al/Cu.


CTA-ID : 2054545
Was this helpful?
What can we do to improve the information ?