Technical FAQs

Ask a Question

Are the IEC D-Line contactors SEMI F47 compliant?

 Identifying D line contactors compliance

Product Line:
Tesys D contactors

Products sold and used in the United States
 SEMI F47 compliance required
D-Line contactors with AC coils are not SEMI F47 compliant.

D-Line contactors with DC coils are SEMI F47 compliant and perfect for EMO contactor applications. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.

CTA-ID : 2054183
Was this helpful?
What can we do to improve the information ?