Technical FAQs

Ask a Question

Are the QOU16150JBAF, QOU16150BAFB, QOU16150BALB or QOU16150BARB Jumper Bar Assembly suitable for both single phase or three phase?

Issue:
Application:

Product Line:
QOU Jumper Bar Assembly

Cause:
Clarification of application

Resolution:
These QOU Jumper Bar Assemblies are only suitable for use single phase voltage systems.


CTA-ID : 2053950
Was this helpful?
What can we do to improve the information ?