Technical FAQs

Ask a Question

Is a DTU362AWK dual rated for NEMA 3R and NEMA 12 applications?

The DTU362AWK is rated for NEMA 3R or NEMA 12 applications. For NEMA 3R applications remove the drain screw in the bottom endwall.

CTA-ID : 2054511
Was this helpful?
What can we do to improve the information ?