Technical FAQs

Ask a Question

What is the Main Lugs Only kit for a QO342M200?

Issue:
Application/Selection

Product Line:
QO Load Center

Environment:
Convert MB to MLO

Cause:
Clarification

Resolution:
Use QOL3225 to convert the QO342M200 to a Main Lugs Only loadcenter....and a KFP filler plate (2/5/15 update: KFP is now obsolete and no longer available).


CTA-ID : 2054459
Was this helpful?
What can we do to improve the information ?