Technical FAQs

Ask a Question

Are the 9080K line of terminal blocks, including unit construction type blocks obsolete? What is the recommended <br />replacement?

The 9080G blocks will fill most applications, and will fit on the same 9080GH track.
The 9080 unit construction blocks will covert to the 9080LBC power distribution blocks.
See the Digest or catalog number 9080CT9601for conversion options available.



CTA-ID : 2054370
Was this helpful?
What can we do to improve the information ?