Technical FAQs

Ask a Question

What is the wire range of the lugs on the 82445R?

The 82445R will accept qty 1, 1/0 to 600kcmil or qty 2, 1/0 to 300kcmil Al/ Cu.


CTA-ID : 2054180
Was this helpful?
What can we do to improve the information ?