Technical FAQs

Ask a Question

9080LBFA is being obsoleted, is there going to be a replacement?

We introduced the 9080LBFA blocks to meet the feeder spacing requirements of UL Standard 1953. We have learned that the requirements are not going to be enforced. The 9080LBFA blocks are larger and are set at a higher price point than the alternative blocks (9080LBA & 9080LBC) and have not gained a sufficient foot-hold in the market. As a result, we are withdrawing the blocks from the market effective May 26, 2010.


CTA-ID : 2054184
Was this helpful?
What can we do to improve the information ?