Technical FAQs

Ask a Question

How does the QO Intelligent load centers allow load shedding with the branch breakers?

Issue:
Product design feature

Product line:
QO Load centers

Environment:
Product functions

Cause:
Application

Resolution:
NOTE: All the QO ILC catalog numbers are obsolete, NLA with NO replacement.

Load Shedding occurs when the QO-PLILC branch breakers receive input from the generator, opening and closing the contacts in these breakers.

 
Was this helpful?
What can we do to improve the information ?