Technical FAQs

Ask a Question

Are the arc fault breakers rated only up to 1000 watts of load?

They are rated to a maximum of 1000 watts for dimming loads. On non-dimming loads a 20A AFI breaker is rated up to 1920 watts continuously.

Updated 2/15/2012 - We have successfully tested to 1920 watts of dimmable lighting loads.

CTA-ID : 2054455
Was this helpful?
What can we do to improve the information ?