Technical FAQs

Ask a Question

What is the difference between a QO330M125 and a QO330MQ125 load center?

Issue:
Product Features

Product Line:
QO LC

Cause:
Clarifying feature differences

Resolution:
The QO330MQ125 (Series S03) has a new style of main circuit breaker installed. The KDL main circuit breaker supplied in Series S01 panels has been replaced by the QDL main circuit breaker. The new style load center requires cover QOC342MQF (flush application) or QOC342MQS (surface application).
The QDL main breaker will not fit in the older style QO330M125 load center.


CTA-ID : 2054369
Was this helpful?
What can we do to improve the information ?