Technical FAQs

Ask a Question

What is the temperature rating on the lugs for the QDA breaker ?

The temperature rating is 75 deg C. The breaker and lugs are tested as a system using 75 deg wire.


CTA-ID : 2054136
Was this helpful?
What can we do to improve the information ?