Technical FAQs

Ask a Question

How many characters can be engraved on the NQ panel name plate?

Issue: How many characters can be engraved on the NQ panel name plate? Product Line: Panelboards. Environment: Products sold in the United States. Cause: Product featues. Resolution: The standard name plate is 1 X 3.5 inch, it will accept 3 lines, 18 characters per line and the letters are 0.18`` high.
The oversized name plate is 2 X 6 inch, it will accept 3 lines, 15 characters per line and the letters are 1/2`` high.


CTA-ID : 2054118
Was this helpful?
What can we do to improve the information ?