Technical FAQs

Ask a Question

Is the PowerBus rated for a Nema 4 application.

No, the straight sections and fittings for PowerBus are rated for NEMA 1 applications but are also protected to IP54 as standard.


CTA-ID : 2054242
Was this helpful?
What can we do to improve the information ?