Technical FAQs

Ask a Question

What is the UL file number in which the Trenchduct is listed?

Square D`s Trench Duct is a UL listed product and is in compliance with UL884 and Article 354 of the NEC.
UL file number is E30049


CTA-ID : 2054231
Was this helpful?
What can we do to improve the information ?