Technical FAQs

Ask a Question

Can the LUB12 with a LUCA*** control unit operate at 50hz ?

Yes , the product control rating is 50/60Hz, the frequency limits are 40-60hz


CTA-ID : 2054376
Was this helpful?
What can we do to improve the information ?