Technical FAQs

Ask a Question

What are the repair parts for the H221DS, series F5? (may be shown as F05)<br />

The repair parts for the H221DS, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 40566-427-50 (arc suppressor not included)
-Load Base Assembly - 40566-408-50
-Line & Load Base mounting screw - 40205-160-01 (3 for line & 2 for load)
-Arc Suppressor Assembly - 40560-018-01
-Arc Suppressor mounting screw - 40205-145-01 (1 required)
-Lug Assembly - CL0306F (includes 6 lugs)
-Mechanism Assembly - 40566-107-50 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 40566-998-50
-Cover Interlock Defeat Coupling - 40566-997-50
-Handle Assembly - 40566-994-50 (also recommend replacing Lockplate Gaskets)
-Lockplate - 40566-932-01 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 40503-228-02 (2 required)
-Lockplate mounting screw - 21949-000-01(2 required)
-Ground Lug - 40251-016-52 - (2 total required)
-Ground Lug Mounting Screw - 40205-135-03
-Fuse Pullers - FPK03 (1 required for switch)



CTA-ID : 2054761
Was this helpful?
What can we do to improve the information ?