Technical FAQs

Ask a Question

Can the operating handle of a 82455 Double Throw safety switch be padlocked in the ON or OFF position??

Lock OFF:
Provision to lock the operating handle in the OFF position is standard on this device.
Lock ON:
Provision to lock the handle in the ON position is also standard (subject to local code regulations - consult local authorities for interpretation).

CTA-ID : 2054074
Was this helpful?
What can we do to improve the information ?