Technical FAQs

Ask a Question

Is the connector with screw terminals for the P frame motor operator replaceable?

The connector is installed as part of the electrically operated mechanism and does not come with the motor or coils.

The parts are not available as replacement parts.


CTA-ID : 2054201
Was this helpful?
What can we do to improve the information ?