Technical FAQs

Ask a Question

How can input and output parameters be displayed in Custom units?

An example and General instructions are given below.

Example: A 0-10V Torque Refence assigned to AI1 needs to be displayed as 0-100% signal.
1. Main menu - Display config - User parameters - Parameter selection
2. After clicking on Parameter Selection, the display takes you to the Drive Menu.
3. Select Monitoring - Torque Reference; click enter to select that parameter. Then press esc and the display will take you back to User Parameters.
4. Select Customized Selection; press enter and you will see the parameter(s) you selected. Highlight it and press enter.
5. User name -- rename the parameter to what you select
6. Unit -- select %
7. Multiplier -- set for 10
8. Press esc until you get back to the main menu. Select Monitoring Config - Param. Bar Select; select the parameter you just created and it will show on the display screen.

General Instructions:
1. Main menu - Display config (menu 7)- User parameters (menu 7.1)- Parameter selection
2. After clicking on Parameter Selection, the display takes you to the Drive Menu (menu 1).
3. Select Monitoring (menu 1.2) - Motor Speed; click enter to select that parameter. Then press esc until you`re back at User Parameters (menu 7.1).
4. Select Customized Selection; press enter and you will see the parameter(s) you selected. Highlight the one you want to customize and press enter.
5. User name -- name the parameter as desired using the F1, F2, and F3 function keys.
6. Unit -- select desired units from the list
7. Multiplier -- set as required for the scaling
8. Press esc until you get back to the main menu.
9. Select Monitoring Config. (menu 6) - Param. Bar Select (menu 6.1) for display on top line; for display on the Main display, select Monitor Screen Type (menu 6.2) Choices are: Display value type: digital (2 max), bar graph (2 max), and list (5 max).
10. Select the parameter you just created and it will show on the display screen.


CTA-ID : 2053996
Was this helpful?
What can we do to improve the information ?