Technical FAQs

Ask a Question

What are the repair parts for the DTU363DS, series F5? (may be shown as F05)<br />

The repair parts for the DTU363DS, series F5 (F05) are as follows. No other parts are available.
-Line Base - 40566-247-50 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately).
-Line Base mounting screws - 40205-151-01 (requires 3 per line base).
-Arc Suppressor Assembly - 40566-355-50 (requires 1 per line base).
-Arc Suppressor mounting screw - 40205-145-01 (requires 1 per arc suppressor).
-Wire Assembly- 40566-218-50 (requires 1 per phase. Includes cable factory connected mechanical lug at one end and at other end a crimped connector. Use mounting screws of line and load lugs.)
-Line and Load Lug Assembly - CL10F (includes 6 lugs)
-Line, Load Lug mounting screw - 40205-142-02
-Ground Lug - 40251-018-51 (per lug).
-Ground Lug mounting screw - 40205-135-03
-Switch Mechanism - 40566-469-50 (each for upper and lower).
-Linkage Assembly - 40566-653-50 (links together upper and lower switch mechanisms). Also replace linkage assembly rubber gaskets.
-Linkage Assembly Rubber Gaskets - 40503-228-01 (3 total required)
-Linkage Assembly mounting screws - 21949-000-01 (requires 7).
-Handle - 40566-888-50
-Lockplate - 40566-895-01
-Lockplate mounting screws - 21949-191-21 (requires 2).



CTA-ID : 2054765
Was this helpful?
What can we do to improve the information ?