Technical FAQs

Ask a Question

XD4PA12: Are the contacts included?

Issue:
XD4PA12:  Are the contacts included?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
Yes. It is provided with 1 normally open contact per direction.


CTA-ID : 2054140
Was this helpful?
What can we do to improve the information ?