Technical FAQs

Ask a Question

What are the spare parts for the EE112TxxH (and all 112.5 kVA 150 C rise k1rated) transformers?<br />

The spare parts for the EE112T65H are:
WS364 - Weathershield
CMB364 - Ceiling mounting bracket
4305512501 - Top cover
4300507404 - Front (When replacing front panel, specify the transformer part number and ``with nameplate and labels`` on order)
4300507404 - Rear
43005512601 - Sides (ends)
4305512450 - Base


CTA-ID : 2053967
Was this helpful?
What can we do to improve the information ?